cancel
Showing results for 
Search instead for 
Did you mean: 

Debug the Audio_SD example with Cradle mounted

frnt
Senior

Hello to everybody,

I bought the bluecoin evaluation kit and I'm interested in logging audio data in SD, similarly to the Audio_SD example.

I have tried the Demo, downloading the .bin using the SWD cable from the nucleo board. Then removed the CoreSystem from the CoinStation and put it on the Cradle.

This is find for the final applications. However, I was wondering if there is a way to debug the application not just downloading the .bin using Stlink.

Ok I can use the SWD cable but I have to put to CoreSystem on the Cradle and doing that I cannot debug the writing on the SD card.

Is there a solution to the debug the whole application (SD included) ?

Thanks.

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @frnt​ 

can we refer to this thread for the topic of this topic?

-Eleon