cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L7CX clean room requierment

SabinMimulici
Associate

Hello,

We are investigating the VL53L7CX presence detection ToF sensor. In the datasheet its mentioned it needs to be mounted in a clean environment "The customer is advised to use a clean assembly process until a
protective cover glass is mounted." and the application note TN1532 "Recommendations for assembling dToF sensors without liners in an environmentally clean place" - states that the sensors should be mounted in a clean environment grade 1000.  Our manufacturer dose not have a 1000 grade clean room but he has 10000 grade. 

What would be the consequences of mounting the sensor in an 10000 grade environment ?

 

Thank you very much! 

 

1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

This is a hard question to answer. ST of course has over-specified the requirement. But it's out of caution that we do this. We know the sensor will not work as well if you get debris in the openings.

As a practical matter it would depend on time. If you did the wave soldering and placed the cover over the chip soon after it comes out of the oven, you would be fine with a 10,000 grade cleanroom. 

But if you soldered them and left them for a week or two off in the corner somewhere, you would possibly have a problem. 

I would suggest that if you could keep them as clean as you can within reason, for a short a time as possible you would be fine. 

After all, I have some VL53L7 boards sitting on my desk in an open office and they work fine after months of sitting there. But I only have one or two and you potentially have thousands. And if mine fail, I can just get another, but you will have un-happy customers.

Set up a process where you pull the liner off JUST prior to putting on the protective cover glass and be as clean as you can. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

2 REPLIES 2
John E KVAM
ST Employee

This is a hard question to answer. ST of course has over-specified the requirement. But it's out of caution that we do this. We know the sensor will not work as well if you get debris in the openings.

As a practical matter it would depend on time. If you did the wave soldering and placed the cover over the chip soon after it comes out of the oven, you would be fine with a 10,000 grade cleanroom. 

But if you soldered them and left them for a week or two off in the corner somewhere, you would possibly have a problem. 

I would suggest that if you could keep them as clean as you can within reason, for a short a time as possible you would be fine. 

After all, I have some VL53L7 boards sitting on my desk in an open office and they work fine after months of sitting there. But I only have one or two and you potentially have thousands. And if mine fail, I can just get another, but you will have un-happy customers.

Set up a process where you pull the liner off JUST prior to putting on the protective cover glass and be as clean as you can. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

Thank you very much for your fast reply and clear answer.

Cheers,

Sabin