2021-12-05 3:41 AM
2021-12-10 7:37 AM
Hi, in the AN5040 the following is reported:
The step count is not reset to zero when the accelerometer is configured in Power-Down or the pedometer is disabled; it can be reset to zero by setting the ****_RST_STEP bit of the CTRL10_C register to 1. After the counter resets, the ****_RST_STEP bit is not automatically set back to 0.
This means that you have to configure that bit to 1 in order to reset the step counter (or power off the device), but if you want to use it after this reset, you have to turn manually that bit to 0. Is this your doubt?
2021-12-10 7:37 AM
Hi, in the AN5040 the following is reported:
The step count is not reset to zero when the accelerometer is configured in Power-Down or the pedometer is disabled; it can be reset to zero by setting the ****_RST_STEP bit of the CTRL10_C register to 1. After the counter resets, the ****_RST_STEP bit is not automatically set back to 0.
This means that you have to configure that bit to 1 in order to reset the step counter (or power off the device), but if you want to use it after this reset, you have to turn manually that bit to 0. Is this your doubt?
2021-12-14 2:13 AM
Hi @Community member ,
did @DSull.3 helped you with your issue?
-Eleon
2021-12-14 3:47 AM
Hi.
I got the help I needed , issue is resolved.
Thanks