2018-02-15 7:29 PM
I am trying to develop a driver for my project which uses this Accelerometer / e-compass and while there is plenty of information for me to get something working, it is missing some information and some information is just not correct.
I would specifically like to add support for high pass filtering but I have no idea what HPCF[2:1] does - there was mention by someone at Pololu that the LSM303DLM datasheet has this information but can I fully trust that these filter coefficients are the same?
There was also mention of 2 data ready signals as quoted from the revision 2 datasheet on page 16
The LSM303DLHC features two data-ready signals (RDY) which indicate when a new set of
measured acceleration data and magnetic data are available, therefore simplifying data synchronization in the digital system that uses the device.There is only one externally accessible DRDY signal, however there are two interrupt lines. There also doesn't seem to be any information on the DRDY signal. Is this asserted when there is data available on the X,Y,Z registers, how about FIFO? Magnetometer data?
I can probably deduce the DRDY pin use from selective disablement of the accel/mag so I am not too concerned with that.
So my questions are:
Thanks all for your time
#lsm303dlhc2018-02-16 1:34 AM
1. No there is no errata to the datasheet.
2. I would not recommend you to use other datasheet, even it the devices looks similar there could be differences.
Concerning the high pass filter cut-off frequencies (HPCF[2:1] bits) I can try to get the values.
The DRDY pin is data ready signal from the magnetometer only.
The INT1 and INT2 pins can be configures using CTRL_REG3_A (22h) and CTRL_REG6_A (25h) registers.
Where you can select which signals will be available on the pins (Data ready from accelerometer, threshold interrupt, FIFO watermark, ...)
I would also like to mention, that the LSM303DLHC is not recommended for new design, there are newer and better sensors.
2018-02-16 5:54 AM
Hi Miroslav
I wouldn't normally choose a device with a NRND status if I was designing something from the ground up but seeing as though this is the only chip I have at the moment for experimentation, I thought I would give it a go.
As for using the the other datasheet for the filter coefficients, I was hoping the same filter internals were being used in the IC to save on re-design costs.
Thanks
2018-02-23 5:02 AM
Here are the cut-off frequencies for high pass filter:
2018-02-24 2:11 PM
Thanks for taking the time for finding this information Miroslav
Much appreciated
Kind regards
Adam