2013-12-23 06:01 AM
I would like to configure both the CS43L22 Audio DAC and the LSM303DLHC MEMS accelerometer to be used simultaneously. From what I have seen on the documentation, it seems that both of these devices are connected to I2C1.
Is it possible to reconfigure one of these devices to use I2C3?Or maybe to disconnect I2C1 from the Audio DAC after the control information is sent, so that the information from the accelerometer doesn't interfere with the audio signal?ThanksJoe #stm32f4-cs43l22-lsm303dlhc2014-01-10 09:39 AM