cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSV320X: Confirmation on Free-Fall Interrupt Mapping (INT10)

Ahilesh_Krishna
Associate

Hello Team,

We are using SensorTile.box Pro with the STEVAL-MKI251A (LSM6DSV320X) adapter board and MEMS Studio version 2.2.0. Flashed the sensor tile box pro with the DataLogExtended.bin firmware which is available in the MEMS Studio

We have logged accelerometer Low-G and High-G data at 1.9 kHz. Additionally, we enabled and monitored interrupts from INT1 to INT10 during the test.

We observed that only INT10 shows an output value of 1, while all other interrupts remain inactive.

Could you please confirm from your side whether INT10 = 1 corresponds to the Free-Fall interrupt for this sensor configuration? Also, kindly let us know if this behavior is expected when using MEMS Studio 2.2.0 with SensorTile.box Pro and the STEVAL-MKI251A.

Thank you for your support.

Best regards,
Ahilesh

0 REPLIES 0