cancel
Showing results for 
Search instead for 
Did you mean: 

How to set high-g threshold for LSM6DSV320X

Muffss18
Associate

Hi,

We are using LSM6DSV320X for our product and want to generate interrupt when high-g is detected. In which register do we need to set the threshold so that the interrupt is generated at or above that value.

2 REPLIES 2
Federica Bossi
ST Employee

Hi @Muffss18 ,

You can refer to AN6119, especially in section 5.7 you can find all the information you need.

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Federica Bossi,

 

Thank you for your response.

As mentioned earlier, Section 5.7 does not provide details on how to configure the High-G shock threshold for interrupt generation. We would like to set a specific High-G shock threshold such that, when our device experiences acceleration beyond that level, the sensor should trigger an interrupt.

Could you please guide us on how to configure different threshold values for High-G shock detection?