cancel
Showing results for 
Search instead for 
Did you mean: 

Marking of LSM6DSVTR

VenusY
Associate

 

LSM6DSVTR is marked V3,

Does it change the DC format from YWW to Y or another format? What does "4" mean?

Thank you.

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @VenusY, to the community!

The format is still the same, i.e. YWW. For reasons unknown to me, only the year appears to have been marked on your device. It would be helpful if you could insert a more legible photo, or at least zoom in a little further with your camera.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Shot20251224173918997.jpg

Please check the photo, thank you.

Unfortunately, I am unable to read the 2D code due to strong reflections caused by the rough surface. You are welcome to send me a photo of the label on the packaging/bag via PM, but please do not post it here in the public community to prevent misuse.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.