2023-10-23 9:08 AM
Hello,
For the asm330lhhx device, when does the scale value change and get set? I am trying to determine if the scale factor needs to be checked only once at power up or continually while reading the raw x, y, and z values for both the gyro and the accelerometer.
In Linux Terminal, the scale and raw values show up as the following for the x component of the gyro:
in_anglvel_x_scale
in_anglvel_x_raw
I plan to read the scale once and the raw value continuously. But if the scale value changes, then I need to read both continuously. Please confirm how they work as the datasheet was not clear on this.
Thank you!
Solved! Go to Solution.
2023-10-23 10:19 AM
I see now that you can set the scale value yourself. Please close this issue.
2023-10-23 10:19 AM
I see now that you can set the scale value yourself. Please close this issue.