cancel
Showing results for 
Search instead for 
Did you mean: 

ASM330LHB fault detection in dynamic conditions

Deviprasad Bokkisam
Associate II

1.Shall ASM330LHB able to detect the sensor(Gyro and Accelerometer) fault in dynamic(not stationary) conditions and send the information to Host?. Self test will give fault information but it is applicable only in stationary conditions.

2.If above is not possible ,can you please suggest any algorithms to detect the faults in IMU?

1 REPLY 1
Federica Bossi
ST Employee

Hi @Deviprasad Bokkisam ,

The self test works only in static conditions, you can detect the faults when it is in a steady state condition.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.