2024-08-12 4:58 AM
Hi,
I am using ASM330LHB in my project. ASM330LHB has only built self test which can only executed during power on to see ASM330LHB is healthy or faulty? But during runtime (device working in dynamic conditions) there is no way to find ASM330LHB is healthy or faulty?
1. Please suggest a method to find ASM330LHB is healthy or faulty during runtime?
2. Is ASM330LHB is fully calibrated against over its temperature range?
Thanks in advance,
Pavani.
2024-09-02 8:05 AM
Hi @Pavani ,
The self test works only in static conditions.
I confirm that ASM330LHB is calibrated over the entire temperature range.
2024-09-11 11:34 PM
Hi, Thank you for your reply. How many times we can perform self test (in static condition) for ASM330 in its lifetime? Is there any limit OR can we perform self test unlimited times? If there is any limit please mention the count.
Thanks in Advance,
Pavani