cancel
Showing results for 
Search instead for 
Did you mean: 

Any problem if the NC pin in LIS3DH is connected to GND?

Vu Tran1
Associate
Posted on March 05, 2018 at 07:46

In many other IC I saw NC pin being connected to GND. However, in LIS3DH, it is not recommended that we should leave it floating or connect it to GND. So I'm wondering if there is any problem if we connect the NC pins to GND?

1 REPLY 1
Miroslav BATEK
ST Employee
Posted on March 06, 2018 at 09:58

In case of LIS3DH you can connect the NC pins 2, 3 to ground. It is not a problem.