2021-11-18 05:18 PM
Hi genius,
I need help to implement SDI-12 in STM32G081. Im using STMcubeIDE. Before this, I have tested the SDI-12 sensor which is soil moisture sensor with arduino maker nano and it works. Its not a big deals since the example is provided. I tried to plot the code from arduino into cubeIDE but Im not an expert programmer. I need help to implement in STM32. There are no such SDI-12 in cubeMX but Im sure you can provide example in cubeIDE. Please help me.
Thanks in advanced.
2021-11-19 06:17 AM
Probably the same topic as there?
Regards
/Peter