2020-11-23 5:05 AM
Hi!
I am using Algobuilder and I tried to use a flexible number of properties (like for example in the "Graph"). Although undocumented, I saw in the library for the display that there are <DisplayDependency> and <DisplayCondition> tags. I tried to use them in a custom block, but unfortunately the user interface is not automatically updated when changing the number and the input fields for the properties do not appear.
It is working if I set a value and reload the entire functin block design or the library in algobuilder.
Is this a bug or is this feature simply not supported by custom made blocks?
Best wishes,
Dominik
Solved! Go to Solution.
2020-11-23 6:40 AM
Hello Dominik,
we din't expect this will be used by users custom made blocks.
But it should work except the properties are not automatically updated. You need to deselect the function block and select it again to refresh the properties table.
We will try fix it in the next version of AlgoBuilder.
2020-11-23 6:40 AM
Hello Dominik,
we din't expect this will be used by users custom made blocks.
But it should work except the properties are not automatically updated. You need to deselect the function block and select it again to refresh the properties table.
We will try fix it in the next version of AlgoBuilder.