X-NUCLEO-PLM01A1 + STEVAL-XPLM01CPL not working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-17 8:50 AM
Hello
i have a pair of X-NUCLEO-PLM01A1 plugged on two NUCLEO-G071RB that communicate in P2P mode, one is master board and one is slave board
i have adapted the example provided by ST to work on this boards:
https://www.st.com/en/embedded-software/x-cube-plm1.html
The communications using a 2 wire to connect the CN1 on the X-NUCLEO-PLM01A1 is completely functional
BUT
if i try to connect the two board using two STEVAL-XPLM01CPL is not working anymore
i connect the two high voltage side on the 230VAC 50Hz same socket and the two low voltage side to the respective X-NUCLEO-PLM01A1
there is some modification to do on the example or should be work?
anyone have the same issue ?
Solved! Go to Solution.
- Labels:
-
Power Line Communication
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-20 1:12 AM
hello, sorry for the delay but i made some test.
surprisingly now work in every setup!
i think there was a bad connection that now is fixed.. its the only explanetion i have
i will make some test also at home to test that setup but today in the building is working perfectly.
i will share with you the oscilloscope image of the now working setup:
thank you for your help!

- « Previous
-
- 1
- 2
- Next »