2018-05-10 5:35 AM
Hi,
My device is Bluetooth LE peripheral that is based on BlueNRG-2 and STM32 connected via SPI.
I would like to present some measurement data in SCAN_RSP to central devices.The measurement is performed every 1 second and in this period I update scan_rsp data by:
hci_le_set_scan_response_data()
The data that I pass to above function has following format:
0: 22 - AD_Len1: 0xFF - AD_Type = MANUFACT_SPEC.2-23: custom_data[22] - AD_Data - my measurements
In my central device I receive only about 30% of correct SCAN_RSP, other have empty data:
11662 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -53 dBm :: [24]: 16 ff 01 10 99 1c 70 00 15 00 80 03 80 fe c0 c0 00 00 6c 01 00 17 01 00
14757 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [0]:
19177 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [24]: 16 ff 01 10 bb 93 71 00 15 00 80 03 40 ff 40 c1 00 00 6c 01 00 17 01 00
22272 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [0]:
24485 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 dd 0a 73 00 15 00 40 03 00 ff 80 c0 00 00 6c 01 00 17 01 00
27532 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [0]:
29742 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 ff 81 74 00 15 00 80 03 80 ff 40 c1 00 00 6c 01 00 17 01 00
34999 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 11 f9 75 00 15 00 40 03 c0 fe 00 c1 00 00 6c 01 00 17 01 00
38047 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [0]:
40254 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [0]:
41363 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -52 dBm :: [24]: 16 ff 01 10 33 70 77 00 15 00 80 03 00 ff 00 c1 00 00 6c 01 00 17 01 00
44410 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [0]:
46620 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -54 dBm :: [0]:
47725 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 55 e7 78 00 15 00 80 03 40 ff c0 c0 00 00 6c 01 00 17 01 00
50771 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -59 dBm :: [0]:
54086 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -51 dBm :: [24]: 16 ff 01 10 77 5e 7a 00 15 00 40 03 40 ff c0 c0 00 00 6c 01 00 17 01 00
57131 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -61 dBm :: [0]:
59342 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 99 d5 7b 00 15 00 40 03 c0 fe 40 c0 00 00 6c 01 00 17 01 00
62389 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [0]:
64600 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [0]:
65705 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 bb 4c 7d 00 15 00 c0 03 40 ff 80 c1 00 00 6c 01 00 17 01 00
68802 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -60 dBm :: [0]:
71012 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 dd c3 7e 00 15 00 80 03 80 ff 00 c1 00 00 6c 01 00 17 01 00
74109 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -61 dBm :: [0]:
76319 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -56 dBm :: [0]:
77425 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -55 dBm :: [24]: 16 ff 01 10 1f 3b 80 00 15 00 40 03 40 ff 40 c1 00 00 6c 01 00 16 01 00
80519 0> SCAN_RSP, xx:xx:xx:xx:xx:xx RSSI -61 dBm :: [0]:
Why data are empty for some SCAN_RSP?
Kind regards,
Piotr #scan_rsp #bluenrg-2Solved! Go to Solution.
2018-05-10 9:29 PM
My mistake.
I overlooked that after each connection I call SetDiscoverable where was setting SCAN-RSP data to null.Regards,
Piotr
2018-05-10 9:29 PM
My mistake.
I overlooked that after each connection I call SetDiscoverable where was setting SCAN-RSP data to null.Regards,
Piotr