2015-07-01 01:00 AM
2015-07-07 06:45 AM
2015-07-07 06:55 AM
# ip_ipaddr = 0.0.0.0
# ip_netmask = 0.0.0.0
# ip_gw = 0.0.0.0
# ip_dns = 0.0.0.0
into status/config are ok?
2015-07-07 07:08 AM
# ip_ipaddr = 172.31.12.1 # ip_netmask = 255.255.255.0 # ip_gw = 172.31.12.1 # ip_dns = 208.67.222.222
2015-07-07 08:16 AM
Variables are ok.
I tried (a few months ago) in STA mode, but never in miniAP. I expect it should work, since IP addresses are delivered in the same way!Give me some time to perform a couple of tests...Sorryjerry2015-07-10 12:37 AM
Tests confirmed your issue.
Opened a ticket for investigation/solving.Sorry for thisjerry2015-07-10 02:51 AM
2017-01-26 03:38 PM
Thanks from me for this info,
. I had pretty much the same issue, trying to join my WPA2 network.Setting aut_type to 0 made it possible:
+WIND:2:Reset+WIND:1:Poweron (150410-c2e37a3-SPWF02S)+WIND:13:ST SPWF01SA2 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.+WIND:3:Watchdog Running+WIND:46:WPA: Crunching PSK...+WIND:0:Console active+WIND:32:WiFi Hardware Started+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:xx:xx:xx:43:02:94+WIND:25:WiFi Association with '***_wireless' successful+WIND:51:WPA Handshake Complete+WIND:24:WiFi Up:x.x.1 �?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
So my question now is: Your post below infers that setting auth_type to zero makes the module use WEP encryption? That cannot be the case because my wifi is definitely using WPA2 only - which seems to be confirmed by the WPA lines above.
If I set auth_type to 1, though, I get his output:
+WIND:2:Reset+WIND:1:Poweron (150410-c2e37a3-SPWF02S)+WIND:13:ST SPWF01SA2 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.+WIND:3:Watchdog Running+WIND:0:Console active+WIND:32:WiFi Hardware Started+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:xx:xx:xx:xx:xx:xx+WIND:45:Dot11 AuthIllegal 1/2+WIND:75:Rejected Association (0xD) �?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
The config producing the error:
# Dumping All Configuration Keys:# nv_manuf = ST# nv_model = SPWF01SA2# nv_serial = 2215P15051# nv_wifi_macaddr = 00:80:E1:B5:AF:25# blink_led = 0# wind_off_low = 0x00000000# wind_off_medium = 0x00000000# wind_off_high = 0x00000000# user_desc = anonymous# escape_seq = at+s.# localecho1 = 0# console1_speed = 115200# console1_hwfc = 1# console1_enabled = 1# sleep_enabled = 0# standby_enabled = 0# standby_time = 10# wifi_tx_msdu_lifetime = 0# wifi_rx_msdu_lifetime = 0# wifi_operational_mode = 0x00000011# wifi_beacon_wakeup = 1# wifi_beacon_interval = 100# wifi_listen_interval = 0# wifi_rts_threshold = 3000# wifi_ssid = xx:xx:xx:xx:5F:77:69:72:65:6C:65:73:73:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_ssid_len = 13# wifi_txfail_thresh = 5# wifi_ht_mode = 0# wifi_channelnum = 6# wifi_opr_rate_mask = 0x00003FCF# wifi_bas_rate_mask = 0x0000000F# wifi_mode = 1# wifi_auth_type = 1# wifi_atim_window = 0# wifi_powersave = 0# wifi_tx_power = 18# wifi_rssi_thresh = 0# wifi_rssi_hyst = 0# wifi_ap_idle_timeout = 120# wifi_beacon_loss_thresh = 10# wifi_priv_mode = 2# wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_key_lens = 00:00:00:00# wifi_wep_default_key = 0# wifi_wpa_psk_raw = xxxxxxxxxxx# wifi_wpa_psk_text = xxxxxxxx# ip_use_dhcp = 1# ip_use_httpd = 1# ip_mtu = 1500# ip_hostname = xx# ip_apdomainname = xx.com# ip_apredirect = firstset.html# ip_ipaddr = 0.50# ip_netmask = 0# ip_gw = 0.1# ip_dns = 0.1# ip_http_get_recv_timeout = 3000# ip_wait_timeout = 12000# ip_dhcp_timeout = 20# ip_sockd_timeout = 250�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Can you explain, please? And is there a reference sheet available somewhere, detailing the error codes?
Thanks a lot!
2017-01-28 04:11 AM
Hi,
using WPA/WPA2, wifi_auth_type must be set to 0. WPA does not support shared authentication.
From Google:
Open System and Shared KeyThe Open System and Shared Key authentication methods use WEP encryption. WEP is not as secure as WPA2 and WPA (Wi-Fi Protected Access). We recommend you do not use these less secure methods unless your wireless clients do not support WPA or WPA2.
Ciao
jerry