2015-07-01 01:00 AM
2015-07-01 01:01 AM
2015-07-01 04:55 AM
Hi Mark,
WIND:45 means there was an error on authentication process.Check shared/open authentication setting between AP and STA.j2015-07-01 05:13 AM
2015-07-01 06:03 AM
2015-07-02 01:12 AM
You can ask for it directly to your local ST support. Faster.
2015-07-02 02:05 AM
Hi, thanks for the reply. ST support faster? Well, I submitted a support request yesterday and so far just got an automated response. I'm sure it would be faster if someone could just read out the low flash into a hex file and post it to the forum.
Cheers, Mark2015-07-02 05:36 AM
Hi Mark,
I don't see support request in the system...Which link did you use?2015-07-02 06:59 AM
TECH008051
. I wish someone would just read the first 0x2800 bytes out of the MCU flash and post the hex to this forum.2015-07-03 12:20 AM
Ticket in on. You should get a reply very soon.
Thanks for patiencej