2016-11-11 06:16 AM
Posted on November 11, 2016 at 15:16
Hi
I want to evaluate BlueNRG using the BlueNRG GUI. My setup is as follows:
I've followed the instructions found in the
and copied Virtual_COM_Port_F401RE.bin the the nucleo drive.
The virtual comm port appears and I can open it from BlueNRG GUI but BlueNRG GUI keeps asking:
''No Firmware detected on the motherboard. Update motherboard Firmware (under Tools menu).''
The proposed firmware installation procedure seems to be targeted at the STEVAL-IDB007V1 BlueNRG-1 development kit and fails with my setup.
Can anyone provide a hint how to get BlueNRG GUI working with the X-NUCLEO-IDB04A1?
Thanks!
2018-02-21 08:59 AM
Excellent, I'm glad that you solved your problem.
2018-02-22 10:55 AM
Posted on February 22, 2018 at 19:55
Can we get the source code for the
<LINK NO LONGER ACTIVE>
https://community.st.com/0D70X000006Su0USAS
It is only binary file.
Thanks