2015-09-15 3:44 AM
Hi,
I tried to connect to a wireless network, which do not broadcast its SSID, with the above mentioned module. I tried as usual: AT+S.SCAN AT+S.SSIDTXT=TestAP AT+S.SCFG=wifi_wpa_psk_text,Test123 AT+S.SCFG=wifi_priv_mode,2 AT+S.SCFG=wifi_mode,1 AT&W AT+CFUN=1 The response after the reset is just the scanning procedure...+WIND:2:Reset
+WIND:1:Poweron (150410-c2e37a3-SPWF02S) +WIND:13:ST SPWF01SA2 IWM: Copyright (c) 2012-2014 STMicroelectronics... +WIND:3:Watchdog Running +WIND:46:WPA: Crunching PSK... +WIND:0:Console active +WIND:32:WiFi Hardware Started +WIND:21:WiFi Scanning +WIND:35:WiFi Scan Complete (0x0) Is there something I've to add to the configuration to get it done? Thanks2015-09-15 8:42 AM
Hi Joe,
Config is ok.I raised your issue. Give me a couple of days...Thanksjerry2015-09-17 5:27 AM
Hi Joe,
problem was confirmed. It will be solved into next FW Release.Thanksjerry2015-09-17 5:28 AM
Hi Joe,
problem was confirmed. It will be solved into next FW Release.Thanksjerry