2021-05-12 11:53 AM
Hello all,
I am attaching the schematics for a PD sink system we have designed and built. Our aim is to get this sink system to accept both PD and non PD type C power supplies and transfer their power to the 'FRONT_PWR' path on our schematics.
Of course a microcontroller is connected and controlling the PD parameters, etc. A few questions:
Thank you very much for your help!
Nir.
2023-08-04 11:20 AM
Hi,
Did you ever get an answer to your question, or figure out what was causing the shutdown?
I have a very similar situation, except at 20V.
2023-08-04 11:46 AM
Hi, I just realized I was using the STUSB4500L part, which is limited to 5V, as encountered by several others on the main thread. It looks like we want the part without the L.