cancel
Showing results for 
Search instead for 
Did you mean: 

STUSB4500L Schematics review + questions

NDvas.3
Associate III

Hello all,

I am attaching the schematics for a PD sink system we have designed and built. Our aim is to get this sink system to accept both PD and non PD type C power supplies and transfer their power to the 'FRONT_PWR' path on our schematics.

Of course a microcontroller is connected and controlling the PD parameters, etc. A few questions:

  1. Is this schematics correct?
  2. If a 15V/3A type C (non PD) power supply is connected, will this system accept it and transfer it's power?
  3. We are having an issue where sometimes when a power supply is connected, the power output will work for a fraction of a second and then shut down. What could be causing this?

Thank you very much for your help!

Nir.

2 REPLIES 2
logic0
Associate

Hi,

Did you ever get an answer to your question, or figure out what was causing the shutdown?

I have a very similar situation, except at 20V.

logic0_0-1691173149383.png

 

logic0
Associate

Hi, I just realized I was using the STUSB4500L  part, which is limited to 5V, as encountered by several others on the main thread. It looks like we want the part without the L.