2022-07-31 7:19 AM
Hello everyone,
I'm trying to write a driver for the ILI9341 display (8 bit parallel mode, not SPI) using the ST HAL. I couldn't get the libraries I found online working, I imagine for the same reason I can't get mine to work. Obviously I have double checked my wiring.
I took an existing Arduino library, stripped a bunch of code away and verified it worked on an Arduino. Then I changed the Arduino specific calls (pinMode, digitalWrite, digitalRead and delay) and converted them into ST HAL equivalent.
The code I attached is supposed to print the display ID (I have removed the auto-generated comments). On Arduino it prints `0x9341` (which is correct), instead the ST version prints `0x1a1a1a1a`.
I'm using a Nucleo 64 STM32L053R8T6 board and STM32CubeIDE. I have attached a screenshot of the configurations of the pins, but I also configure them at runtime (see the functions ILI9341_PrepareDataPinsForWriting and ILI9341_PrepareDataPinsForReading)
I have also added a screenshot of the IDE and of the back of the display.
I understand I'm asking for a lot, it's just that I've spent a week trying to get this stuff working and it's probably something stupid.
Solved! Go to Solution.
2022-08-01 2:10 AM
This is a bit embarrassing, but I did find the issue today.
I had defined the pins to use like this:
#define LCD_RD .port = GPIOC, .pin = 1
Instead of using a number for the pin I should have used the macros:
#define LCD_RD .port = GPIOC, .pin = GPIO_PIN_1
When I was testing the wiring I did find this issue and fix it, except I didn't commit it so i accidentally lost it later
2022-08-01 2:10 AM
This is a bit embarrassing, but I did find the issue today.
I had defined the pins to use like this:
#define LCD_RD .port = GPIOC, .pin = 1
Instead of using a number for the pin I should have used the macros:
#define LCD_RD .port = GPIOC, .pin = GPIO_PIN_1
When I was testing the wiring I did find this issue and fix it, except I didn't commit it so i accidentally lost it later
2023-09-05 8:40 AM - edited 2023-09-05 8:42 AM
Thank you for sharing your code and yhour solution.
I was searching for days for the same thing.
Thanks to your code I was able to find the culprit:
uint32_t portD_data_msk = LL_GPIO_PIN_0 | LL_GPIO_PIN_1 | LL_GPIO_PIN_8 | LL_GPIO_PIN_9 | LL_GPIO_PIN_10 | LL_GPIO_PIN_14 | LL_GPIO_PIN_15;
LL_GPIO_SetPinMode(GPIOD, portD_data_msk, LL_GPIO_MODE_OUTPUT);
see:
__STATIC_INLINE uint32_t LL_GPIO_GetPinMode(GPIO_TypeDef *GPIOx, uint32_t Pin)
{
return (uint32_t)(READ_BIT(GPIOx->MODER,
(GPIO_MODER_MODER0 << (POSITION_VAL(Pin) * 2U))) >> (POSITION_VAL(Pin) * 2U));
}
Is a bad idea as SetPinMode does not! accept multiple pin masks, see RM0090 p281. MODER has multiple bits per IO.