cancel
Showing results for 
Search instead for 
Did you mean: 

STPM33/34 MISO & Insulating barrier

Martin68
Associate II

Hello everyone

I am looking into the STPM33/34. I only want to use 1 SPI bus for both ICs and select it with the SCS.

In the datasheet I cannot see whether the MISO goes into tristate when the IC in question is not active.

I also cannot see any information about the galvanic isolation/barrier.

Can anyone give me information about this.
Thank you in advance.

12 REPLIES 12
Peter BENSCH
ST Employee

Correction to my previous statements and confirmation: both TX (UART) and MISO (SPI) are switched to tristate when the relevant device is deactivated via SCS. Even if it is not explicitly mentioned in the data sheet, several STPM3x can be connected to the same SPI bus and selected via their own SCS.

I have marked the sentence in the previous statements accordingly.

Sorry for the confusion.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

Thanks for the update, this makes it a lot easier.
Thank you again for taking the time to do this.

Best regards,

Martin

Didier HERROUIN
ST Employee

Hello,

The MISO line is in Hi-Z mode when the STPM3x is not selected (SCS at high level).

Just note this limitation in case you use several STPM3x in parallel: 
https://www.st.com/resource/en/errata_sheet/es0591-stpm3x-device-limitations--stmicroelectronics.pdf

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.