cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IDB012V1 / ARDUINO

ljm
Associate III

Hello, please how can I connect a STEVAL-IDB012V1 board with an arduino (if it is possible of course), if not is there a mobile application with which I can connect to this board and retrieve the pressure and acceleration values?

3 REPLIES 3
ljm
Associate III

Hello,

 to program the STEVAL-IDB012V1, i must use STMCube IDE or Keil ?

Andrew Neil
Evangelist III

@ljm wrote:

Hello, please how can I connect a STEVAL-IDB012V1 board with an arduino


Use jumper wires from the headers on the STEVAL-IDB012V1 to the headers of the Arduino ?

AndrewNeil_0-1717074051312.png

Or do you mean how to establish a Bluetooth connection between them?