2019-06-14 12:40 PM
Hi,
I have bought a STEVAL-IDB007V1M so i can learn how to incorporate BLE into my project but im having problems.
The board isn't being picked up on BlueNRG-1 Navigator but it is being picked up on BlueNRG-2 Navigator. - Im not sure if this is a problem?
BlueNRG-2 Navigator allows me to flash and run, so i loaded on the beacon to see if i can find the board on my iPhone, it successfully flashes but i cant see anything on any BLE App.(BLE Scanner, LightBlue)
I have read the other posts that say that the HS_SPEED_XTAL_32MHZ should be 32MHz, but looking at the project code it looks like it is set to that.
Any help would be appreciated.
Kind Regards,
Mike
2020-06-04 06:49 PM
Anyone know the answer to this?
@Thiago REIS