cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IDB007V1M, SPBTLE-1S Not working

MikeP
Senior

Hi,

I have bought a STEVAL-IDB007V1M so i can learn how to incorporate BLE into my project but im having problems.

The board isn't being picked up on BlueNRG-1 Navigator but it is being picked up on BlueNRG-2 Navigator. - Im not sure if this is a problem?

BlueNRG-2 Navigator allows me to flash and run, so i loaded on the beacon to see if i can find the board on my iPhone, it successfully flashes but i cant see anything on any BLE App.(BLE Scanner, LightBlue)

I have read the other posts that say that the HS_SPEED_XTAL_32MHZ should be 32MHz, but looking at the project code it looks like it is set to that.

  

Any help would be appreciated.

Kind Regards,

Mike

1 REPLY 1
PDeck.2281
Associate III

Anyone know the answer to this?

@Thiago REIS​