2018-06-27 11:31 AM
Hi,
I have problem with this wifi module.
After I saved configuration settings in module (act as wifi client) he does not starts at all.
I thought that I destroyed some internal file system structures/module config so I tried to enter into bootloader mode to overwrite firmware and factory settings but without success. It looks like that the module does not response at all.
Information about my module:+WIND: Power On (170111-665d284-SPWF01S)I attached boot sequences screen from logic analyzer.
Does anyone has idea how to start this module or how to make detail diagnosis of this case?
#spwf01sa #wifi-spwf01sa2018-06-28 1:12 AM
OK, I figured out how to enter to factory reset mode:
WLAN_RESTORE_Pin = 1
WLAN_PWR_EN_Pin = 0 ; disable power supply to module
Delay(50)
WLAN_PWR_EN_Pin = 1 ; power up module
Delay(100)
WLAN_BOOT = 0
nRESET = 0
Delay(100)
nRESET = 1
2018-06-28 5:30 AM
Dear,
you should see the power led (GPIO14) lit for a while when deasserting the reset line (or release the reset button on X-Nucleo), this indicates the WiFi module is booting.
In this case please try restoring to factory settings by pulling GPIO0 High at boot.
Regards,
Elio
2018-06-28 7:35 AM
Hi,
sorry, I missed your 2nd comment.
Likely the spwf01's uart was configured with flow control and the flow control line was blocking the spwf01's uart.