2017-09-11 12:03 AM
I'm using STM32 WiFi Cube Extension 3.02 and I see that calling wifi_init restore my module to factory default.
I want the latest AP setup to be saved between module power cycles, if one was set, and by calling wifi init I remove this setup every time the module is started.
I can of course comment it out but I was wondering why it is there from the first place, maybe I'm doing something wrong?
Thanks,
Eyal
#spwf012017-09-12 03:31 PM
Probably because it makes supporting the demo easier. ie a million questions about it not working after configuring it to do X
With modems ATZ is frequently used to load the settings saved with AT&W