2015-10-01 12:51 AM
Hi,
I am broadcasting a small UDP packet once a second through the SPWF01 using AT+S.SOCKON=192.168.1.255,55555,u and AT+S.SOCKW and that appears to work just fine but if I access the SPWF01 web server at the same time to reload some web pages it often dies with a hard fault like this +WIND:8:Hard Fault:TCPIP: r0 2C303035, r1 00000300, r2 00000000, r3 0000FFFF, r12 2000867C, lr 08022E25, pc 08022E3A, psr 61000000 Or the module may just crash, reboot, etc. If I don't do the UDP broadcast, then the module appears reliable. This is very bad as I need to be able to do the UDP broadcast so clients can find the device. Cheers, Mark2015-10-06 03:07 AM
2015-10-06 03:14 AM
Yes, confirm.
I saw after half an hour (SOCKW / F5).SOCKD is ok.I'll try to push this issue solving for next FW release.Sorry for thisjerry2015-10-06 04:44 AM
Hi Mark,
are you waiting for ''OK'' response, before proceeding to next SOCKW?Just to be sure, and safe...ciaoj2015-10-06 05:20 AM
2015-10-06 07:26 AM
Hi Mark,
glad to hear!I agree.Thanksj