2017-01-04 12:52 AM
Hello,
I'am using this module to connecte my borad to Internet.
This module can create a mini AP so a user can connect its laptaop or smartphone to the SPWF01 and configure the WIFI connexion (SSID and pass).
I have no problème to connect to the mini AP with an old WIKO smartphone but I can't connect with a newer smartphone (Huawei P9 lite).
I have also discover a weird thing : If I first connect anything (old WIKO or laptop) to the mini AP, and then try with the P9 lite, it can connect to the mini AP.
thanks for your help.
Marc G
2017-01-05 07:18 AM
Hi,
which version are you using?
Regards
Jerry
2017-01-09 03:01 AM
Hello,
thanks for your help, the version of the firmware of the SPWF01 is 3.4.
regards,
Marc
2017-01-09 07:58 AM
Hi Marc,
please use the latest FW 3.5. If problem is still there, we'll find a way to solve It. Unfortunatelly I have not that device to reproduce the issue.
Thanks
j
2017-01-12 02:43 AM
Ok, I'll try the last firmware.
2017-01-12 05:47 AM
hello,
I can't easily change the firmware of the
SPWF01 on my board. I receives a new edition of my board with, i guess, a newer firmware version for the SPWF01. Below are the tow version extracted from the UART log :
Older board : +WIND:1:Poweron (150410-c2e37a3-SPWF01S)
----> My P9 lite can't connect
Newer board : +WIND:1:Poweron (160129-c5bf5ce-SPWF01S) ----> My P9 lite can connect
Thanks to this test, I assumed that a firmware update of the OLD baord will solve the problem.
Can you confirm my analysis ?
Can you tell me which firmware 3.4 ou 3.5 are my too boards ?
Thanks for your help.
Marc
2017-01-12 10:20 AM
Hi Marc,
Jan 29th 2016 was FW3.5 ->
160129-c5bf5ce-SPWF01S
Apr 10th 2015 was FW3.4 ->
150410-c2e37a3-SPWF01S
Let me know if I can consider closed this issue.
Thanks to you!
jerry
2017-01-13 12:37 AM
Thanks ! This issue can be closed
2017-01-13 02:18 AM
Please use 'Mark Correct' button
2017-02-08 05:30 AM
Hello,
I have solved my problem with my P9 lite phone with the newer firmware version of the module. But with an other smartphone (Nexus 5X android 7) I can' connect to the AP of the module. When I click on the SSID in the WIFI parameter, the smartphone connects to the AP for few seconds then deconnects then reconnects for a few seconds .... and so on. I am working with a module with firmware 3.5 (the last).
thanks for your help.
Marc