Skip to main content
RBair.3
Associate
November 4, 2022
Question

SPSGRFC-915 fails startup sequence after reset

  • November 4, 2022
  • 0 replies
  • 680 views

I'm working with the SPIRIT1 (SPSGRFC-915) radio module, communicating over SPI, and using the provided SPIRIT1_Library. I am stuck after I preform the init sequence, the MC_STATE register keeps coming back with ERROR_LOCK 1, and STATE=2. I never enabled the RCO function so I'm not sure why ERROR_LOCK would be 1, and STATE=2 isn't a valid state on the datasheet, so I am very confused as for what is happening.

void init() { 
SpiritSpiInit();
 
 // restart the radio
 SpiritEnterShutdown();
 SpiritExitShutdown();
 SpiritManagementWaExtraCurrent(); // To be called at the SHUTDOWN exit. It avoids extra current consumption at SLEEP and STANDBY.
 
 // wait for the radio to enter the ready state
 do
 {
 for (volatile uint8_t i = 0; i != 0xFF; i++); // delay for state transition
 // gets stuck here
 SpiritRefreshStatus(); // reads the MC_STATUS register
 } while (g_xStatus.MC_STATE != MC_STATE_READY);
 
...
}

From debugging it looks it gets stuck in SpiritRefreshStatus' while loop

void SpiritRefreshStatus(void)
{
 uint8_t tempRegValue[2];
 
 /* Read the status both from register and from SPI header and exit when they match.
 This will protect against possible transition state changes */
 do
 {
 /* Reads the MC_STATUS register to update the g_xStatus */
 g_xStatus = SpiritSpiReadRegisters(MC_STATE1_BASE, 2, tempRegValue);
 }
 while(!((((uint8_t*)&g_xStatus)[0])==tempRegValue[1] && 
 (((uint8_t*)&g_xStatus)[1]&0x0F)==tempRegValue[0])); 
 
}

I'm using the B-L475E-IOT01A2 board if it helps. Has anyone worked with this device before that can offer some pointers?

    This topic has been closed for replies.