2020-02-08 12:14 AM
Hello. I am making RF beacon based on SPIRIT1 RF IC
I downloaded SPIRIT1 DK, configured for 168MHz based on hardware I have, and written CW mode. But with spectrum analyzer with sweep from DC to 1GHz i can't see anything ( same goes if i select 169MHz with 20MHz span)
I confirmed it does write all registers just like in that application, did confirmed that CW bit is set at 0x1B MOD0 bit 7 with modulation scheme OOK as well as maximum power.
Try sending commands after that, like SPIRIT1_TX or SPIRIT1_LOCKTX, did not helped.
What i am doing wrong ? What I am missing ?