cancel
Showing results for 
Search instead for 
Did you mean: 

Spirit1 dk Contiki

vamsi
Associate II
Posted on October 16, 2014 at 09:07

I started up on SPIRIT1 dk, development kit. I read on net that 6lowpan/contiki is ported on to stm32l+SPIRIT1, and ST promotes that.

But however I'm not able to find downloadable contiki spirit port anywhere. Could anybody please tell me if contiki port for spirit1 dk is available? Or ST guys here can send it.

Thanks and regards,

Vamsi

#contiki-spirit1
3 REPLIES 3
Nickname1920_O
Associate III
Posted on October 16, 2014 at 10:17

Hello,

ST does not have a 6lowpan solution for the mass-market for SPIRIT1. Nevertheless ST is active in the IOT field and thus a solution may be provided in the future.

Regards,

Gaetano

ron239955_stm1_st
Associate II
Posted on October 16, 2014 at 11:03

Hi Chikati

Spirit1 drivers were released as part of Thingsquare-mist, whose source code was being provided on their web site but appears to have been withdrawn. However there are a number of github forks available that continue to provide the code, the last released version of which was 1.1.0, for example https://github.com/ADVANSEE/mist or https://github.com/DJBainbridge/contiki-mist-fork.

STM could perhaps setup their own fork and point people to that.

Best wishes

Ron

vamsi
Associate II
Posted on November 04, 2014 at 06:21

Thanks guys, for your replies.

Hi Ron,

  I'm trying that. But would love to have ST merged it's port into Contiki main branch or at least an active fork by them. For example right now I'm struggling with a serial device implementation for connecting SPIRIT1-DK to internet via a PC. And there ain't nobody to go to :(.

Best Regards,

Vamsi