cancel
Showing results for 
Search instead for 
Did you mean: 

Arduino and X-NUCLEO_IDB04A1

valerio
Associate
Posted on October 21, 2014 at 17:58

Hi, I'm a newby about bluetooth. I bought X_NUCLEO IDB04A1 in order to use it with my Arduino R3. After attaching the shield to Arduino, I expected to find it in the list of available bluetooth device, but no. Do I have to load some special code on Arduino in order to enable the shield? I found no example code. I'm using Debian Wheezy. Thanks a lot.

ps: my bluetooth pc adapter works, I can see my smartphone among the available device.

#x_nucleo-idb04a1 #arduino
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 24, 2014 at 17:02

Currently, ST does not support X_NUCLEO IDB04A1 outside Nucleo Motherboard.

The STM32 Cube firmware X_NUCLEO IDB04A1 is available on the following link:

http://www.st.com/web/en/catalog/tools/PF260705

#

In principle, this software package could be customized, ported in order to support the Arduino platform.

Please notice that this forum is not intended to be used for X_NUCLEO IDB04A1 shield support requests. ST is working on setting up a dedicated forum for this shield and it should be opened by end of this year.

Best regards

Graziella Marchese