2018-04-25 2:18 AM
Hello, I want to make a PCB with a microcontroller STM32L476RG and a Bluetooth module SPBTLE-1S. I plan to use the SPI for the communication beetween the microcontroller and the BLE module but I don't know which pin of this module is used for the interruptions. The older module SPBTLE-RF has a SPI_IRQ pin. Is there a similar pin on the SPBTLE-1S module?
Thanks in advance for your answers.
#bluetooth-low-energy2018-04-27 2:05 AM
DearBaptiste Nguyen,
the
SPBTLE-1S module is based on the BlueNRG-1 chip, which can be used as standalone application processor, able to run the user code for your application along with the BLE stack,
without
the need of an external microcontroller.If you want to use it with an external microcontroller via SPI, just as you did with the SPBTLE-RF module,
you need to load the
DTM_SPI.hex
firmware image on your BlueNRG-1 chip.
Assuming that you have already downloaded the latest version (2.6.0 at the time of this writing) of the BlueNRG-1/2 Development Kit (
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fembedded-software%2Fevaluation-tool-software%2Fstsw-bluenrg1-dk.html
), you can refer to theprocedure described in the 'STM32_SPI_protocol_example.html
'file in the documentation folder of this package (Docs\STM32_SPI_protocol_example_html\STM32_SPI_protocol_example.html
).More details about the SPI protocol used by BlueNRG-1/2 are available in the '
SPI_protocol_specification.html
' file (Docs\SPI_protocol_specification\SPI_protocol_specification.html
).IMPORTANT NOTE
: as you are using the SPBTLE-1S module, please notice that it is based on a32 MHz crystal, whileexamples foundfor BlueNRG-1 are usually configured fora 16 MHz crystal (the one used in the EVAL-IDB007V1 board).Please follow this
https://community.st.com/thread/46418-spbtle-1s-how-to-get-a-ble-connection
for more information about how to rebuild your binaries for 32 MHz.
You can find related information about usage of BlueNRG-1 via SPI by following this
https://community.st.com/thread/44225-firmware-update?commentID=171427#comment
(just remember that in your case you need to rebuild for 32 MHz).
Best regards,
Antonio
2018-05-15 11:48 PM
Thank you for your answer.