cancel
Showing results for 
Search instead for 
Did you mean: 

SPBTLE-1S problem with nucleo L476RG

CDelb.1
Associate

Good morning,

I'm trying to connect the SPBTLE-1S module to my nucleo board, but it seems that the BLE module is not recognized. Using the BlueNRG GUI, I am able to get only the Motherboard FW number, instead the BLE device is not detected. Is it possible that the SPBTLE-1S is not programmed? I've tried also to program the BLE module itself, but without any positive results. Can you provide some detailed guidelines in order to connect the SPBTLE-1S module to my nucleo board and eventually program it with the last FW available?

Thank you in advance.

Carlo

3 REPLIES 3
Winfred LU
ST Employee

It shall be easier just to use STEVAL-IDB007V1M

https://www.st.com/content/st_com/en/products/evaluation-tools/solution-evaluation-tools/communication-and-connectivity-solution-eval-boards/steval-idb007v1m.html

Program the module with DTM firmware application (DTM_UART.hex or DTM_SPI.hex), then you are ready to test with BlueNRG GUI.

Can DTM_SPI.hex be tested through BlueNRG Gui on STEVAL-IDB007V1M?

Yes. Please use the prebuild firmware under STEVAL-IDB007V1M folder.

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.2.1\Firmware\BLE_Examples\DTM\STEVAL-IDB007V1M