2023-02-12 02:17 PM
i did read out the pac number with S2-LP_SigFox_DK_1.7.1 gui and appropriate firmware.
i also did read out the id and it matches the sticker on the board.
in the sigfox backend i can not use the pac to create a new device as it says:
"Invalid PAC code: 26__redacted__ (please contact your device supplier to obtain this code)"
i have paid the subscription fee to enroll that device -> it is not a missing token problem
S2-LP_SigFox_DK_1.7.1 gui says "please go to backend.sigfox.com/activate/STM" when clicking on the id.
calling backend.sigfox.com/activate/STM says that "Free DevKit Connectivity Program Has Ended"
-> not an option to enroll the device that way.
how can i get the hardware to work ~ registered at sigfox / who at stm can give me the right pac number or tell sigfox that the pac number is ok ?