2025-03-29 3:02 PM - last edited on 2025-03-29 11:45 PM by Peter BENSCH
I intend to design a microcontroller circuit with a BTA40-600B RD91 to control the power delivered to a heating resistor (220Vrms, 12Ω, 4KW). I thought about using the MOC3023 to mediate the activation of the BTA40, but I don't know if it is the most suitable optocoupler. Another question is about the snubber circuit. The load is purely resistive, so is a snubber circuit really necessary? Thanks for the help.
Solved! Go to Solution.
2025-03-31 2:13 AM
Welcome @DanielGouvea, to the community!
The output current of the MOC3023 is just sufficient to control the BTA40. However, the BTA40 is not a snubberless TRIAC and therefore requires a snubber circuit. Further information on this and the design of the snubber can also be found in application note AN5114, section 2.4.
Hope that helps?
Regards
/Peter
2025-03-31 2:13 AM
Welcome @DanielGouvea, to the community!
The output current of the MOC3023 is just sufficient to control the BTA40. However, the BTA40 is not a snubberless TRIAC and therefore requires a snubber circuit. Further information on this and the design of the snubber can also be found in application note AN5114, section 2.4.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.