cancel
Showing results for 
Search instead for 
Did you mean: 

Security db problem

jampino
Associate III
Posted on January 05, 2018 at 14:47

Hi all,

I am facing a problem with the security dababase, I am working with BLUENRG-1, I can paired two devices and getting them advertising and create connection, then close the connection and connect again...everything is working fine.

If after all the process I remove the battery from one of the devices and put the batteries back, I can't create a connection again, if I go to the memory position on the bluenrg-1 I can see the address from the device paired there but for some reason I can get them connected again if I do not follow the pairing process.

Any suggestion why that problem could be.

Thank you

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0