cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF04Sx - ip_use_dhcpd

yoann LBY
Senior
Posted on January 04, 2018 at 11:02

hi,

SPWF04Sx + UART + FW1.1.0

en.x-cube-wifi1_firmware_v3.1.0.zip

wifi module is set in miniAP mode. i would like to activate dhcp server. Variable is 'ip_use_dhcpd' = 1 (on).

But dhcp doesn't work!

To set correctly the server dhcp, i should use variable 'ip_use_dhcpc' = 1 (on). The problem is that ip_use_dhcpc is for Client!

I don't know if it's a bug or if i don't understand well server/client dhcp way.

Please Confirm?

file wifi_const.h:

#define IP_USE_DHCP_SERVER                       ''ip_use_dhcpd' 

#define IP_USE_DHCP_CLIENT                          'ip_use_dhcpc'

Thanks

Yoann

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0