2020-07-01 10:07 PM
Hello,
I have testing SigFox Test command for SIGFOX_API_start_continuous_transmission / SIGFOX_API_send_test_frame.
but, Interrupt is not received after Send CMD_TX(0x60).
PLS let me know the procedure for calling this function.
for example
1.ST_RF_API_set_pa
2. SIGFOX_API_set_std_config
....
Thanks, CK
2021-03-03 01:15 AM
Hello,
Are you using SDK 1.7.1?
What is the "sfx_error_t" in the function "SIGFOX_API_start_continuous_transmission"?
What is the hardware used?
Thanks