cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP: Must TX FIFO be filled before calling TX Command?

JKo
Associate III

Is it possible to enter TX mode so it immediately starts sending the preamble and header bytes before any data is in the TX FIFO?

ie. Can the TX FIFO be filled during state transition (READY->LOCK->TX 70us+26us) and preamble time?

Or will the TX Underflow error trigger immediately?

1 REPLY 1
JKo
Associate III

Answering my own question but testing has revealed that it is possible to start TX then write to FIFO.