2019-05-07 05:01 AM
I am using nucleo-l053r8 and i flash it with S2LP_CLI_NUCLEO_L0 firmware. But when trying to open the port: i always get the message "wrong firmware detected. Please click OK to start upgrade procedure..."
I click OK, the firmware is succesfully flashed, but then the popup message is still repeated when trying to open the com port.
How can i open the port successfully?
I have also flashed the board succesfully over mbed interface and over keil microvision. The pop-up message still remains the same when opening the port.
I am using windows 10.
Any help is appreciated.
Solved! Go to Solution.
2019-05-07 06:19 AM
Apparently hardware issues with the board. I took another board and it works.
2019-05-07 06:19 AM
Apparently hardware issues with the board. I took another board and it works.