Skip to main content
EYang
Visitor II
May 8, 2019
Question

S2-LP, SigFox_DK_1.6.0 sample code can't use.

  • May 8, 2019
  • 0 replies
  • 450 views

Hi,

I'm using EVK (STEVAL-FKI868V2), loading the Binaries file to EVK All the command line function is ok. but when I use your sample code:

File Location: 

C:\Program Files (x86)\STMicroelectronics\S2-LP_SigFox_DK_1.6.0\Projects\Projects_Cube\S2-LP_SigFox_DK\SigFox_CLI_Demo_Project\STM32\MDK-ARM\SigFox_CLI_Demo_Project.uvprojx

That will go to "Hardware fault handler" when I type the Command line: "node_open".

is it anything difference between sample code and the Binaries file?

How can I fix this?

thanks,

This topic has been closed for replies.