2021-03-12 11:18 PM
Hi,
I am trying to use subGHz RF modules in my design. I have following questions. It would great if any one could answer these questions. I am trying to build sensor nodes + Gateway. Planning to use mesh over sub GHz.
I have ordered EV kits SPSGRF. I will explore more.
Thanks,
Naveen
Solved! Go to Solution.
2021-03-15 7:34 PM
SPIRIT1 --> SubGHz transceiver generation 1
S2-LP --> SubGHz transceiver generation 2 (S2 for SPIRIT2)
SPSGRF --> SPIRIT1 based module with on-board antenna
SPSGRFC --> SPIRIT1 based module with UFL connector
You will need to certify FCC for the end product.
Contiki stack is software based, which means all these products shall be able to support.
Both SPIRIT1 and S2-LP provide long range transmission with low power.
2021-03-15 11:21 AM
Hello Naveen,
I'm building sensor nodes + gateway too, i use bluenrg + s2lp, i would like to add this about s2lp range :
At the end of 1.1 https://www.st.com/resource/en/application_note/dm00718575-radio-communication-range-estimation-in-ism-band-stmicroelectronics.pdf, the result is 54km, but i can't redo this even with values, is it 10^(126-20*log10(868)-32.44) or am i missing something ?
Thanks,
Andy.
2021-03-15 12:31 PM
Hi Andy,
it looks like that equation is wrong. division of 20 is missing.
it is suppose to be
d = 10 ^[(126-(20*log10(868))-32.44)/20] = 54.88
FSPL′dB= 20×log10d+20×log10868MHz+32.44.
you can refer to above equation or eq 6 in the document.
Naveen
2021-03-15 7:34 PM
SPIRIT1 --> SubGHz transceiver generation 1
S2-LP --> SubGHz transceiver generation 2 (S2 for SPIRIT2)
SPSGRF --> SPIRIT1 based module with on-board antenna
SPSGRFC --> SPIRIT1 based module with UFL connector
You will need to certify FCC for the end product.
Contiki stack is software based, which means all these products shall be able to support.
Both SPIRIT1 and S2-LP provide long range transmission with low power.
2021-03-20 9:24 PM
Thanks Winfred.