2022-07-08 2:47 AM
Hello,
I have a high power consumption during deepstop. The goal is less than 5µA (announced less than 1 in the datasheet).
I removed every other chips on my custom board to found the solution. It's a small board.
When I enter in deepstop mode (without RTC, without any wake-up to test), the current starts at 2-3µA and slowly increases to +-50µA in around 20 seconds. Then the current is stable. We think that it's related with the temperature, if the board is "hot", the starting current is higher.
If I freeze the board, the current change (increase or decrease, it's "random").
I setup PWRC_PUCRx and PWRC_PDCRx according to my board.
Do you know where this issue could come from?
Thank you
Solved! Go to Solution.
2022-08-22 6:04 AM
Hello,
Two things here in my mind
Again the problem you faced is typical of an IO set as input and no pull is present.
Regards
Laurent
2022-07-08 7:03 AM
This may be impractical for you, but if you had a second custom board identical to the one drawing the excessive current, it might be instructive to see if it exhibits the same behavior to rule out a defect in the physical board.
Also, I assume measuring the current is not adversely affecting your results.
If this is a dumb idea or I don't fully understand (likely), ignore it...
2022-07-10 11:49 PM
We have 5 prototype boards with the same behavior. It's not a dumb idea
2022-07-20 7:31 AM
Hello,
From description, really seems no pull are programmed during sleep mode.
Such slow increasing leakage would typically appear if an IO is set as input, physically floating and no pull are programmed.
Please ensure correct pull are set during sleep mode.
In BlueNRG-LP SDK code examples, function BSP_IO_Init() is used to configure all IOs in sleep for optimal power consumption with our STEVAL-IDB011 eval board. It can be reused and adapt for custom PCB.
Regards
Laurent
2022-08-22 1:27 AM
Hello,
Thank you for your response, I already do this but when I check with multimeter, pull down are low state but pull up are floating around 0.03V.
My init code to set IO in sleep mode:
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_SYSCFG_CLK_ENABLE();
HAL_PWREx_DisableGPIOPullUp(PWR_GPIO_A, 0xffff);
HAL_PWREx_DisableGPIOPullDown(PWR_GPIO_A, 0xffff);
HAL_PWREx_DisableGPIOPullUp(PWR_GPIO_B, 0xffff);
HAL_PWREx_DisableGPIOPullDown(PWR_GPIO_B, 0xffff);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO0);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO1);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO2);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO3);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO4);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO5); // Output done in detection
LL_PWR_EnablePDA(LL_PWR_PUPD_IO6);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO7);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO8);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO9);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO10);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO11);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO12);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO13);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO14);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO15);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO0);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO1);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO2); // Input wake up done in detection
LL_PWR_EnablePDB(LL_PWR_PUPD_IO3);
LL_PWR_EnablePUB(LL_PWR_PUPD_IO4);
LL_PWR_EnablePUB(LL_PWR_PUPD_IO5);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO6);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO7);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO8);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO9);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO10);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO11);
// 12 & 13 are not done because XTAL
LL_PWR_EnablePDB(LL_PWR_PUPD_IO14);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO15);
Do you have any idea why pin are not pulled up?
Thank you,
Jean
2022-08-22 2:19 AM
2022-08-22 3:34 AM
Thank I didn't have this doc. I already implemented everything except LSE driving.
during my test, UART and debugger are disconnected.
Part of the schematic that I can share:
IO init:
void BSP_IO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStructure = {0};
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_SYSCFG_CLK_ENABLE();
HAL_PWREx_DisableGPIOPullUp(PWR_GPIO_A, 0xffff);
HAL_PWREx_DisableGPIOPullDown(PWR_GPIO_A, 0xffff);
HAL_PWREx_DisableGPIOPullUp(PWR_GPIO_B, 0xffff);
HAL_PWREx_DisableGPIOPullDown(PWR_GPIO_B, 0xffff);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO0);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO1);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO2);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO3);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO4);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO5); // Output done in detection
LL_PWR_EnablePDA(LL_PWR_PUPD_IO6);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO7);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO8);
LL_PWR_EnablePUA(LL_PWR_PUPD_IO9);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO10);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO11);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO12);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO13);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO14);
LL_PWR_EnablePDA(LL_PWR_PUPD_IO15);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO0);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO1);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO2); // Input wake up done in detection
LL_PWR_EnablePDB(LL_PWR_PUPD_IO3);
LL_PWR_EnablePUB(LL_PWR_PUPD_IO4);
LL_PWR_EnablePUB(LL_PWR_PUPD_IO5);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO6);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO7);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO8);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO9);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO10);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO11);
// 12 & 13 are not done because XTAL
LL_PWR_EnablePDB(LL_PWR_PUPD_IO14);
LL_PWR_EnablePDB(LL_PWR_PUPD_IO15);
// Do nothing when not in sleep
// SWDIO / SWCLK / XTAL0 / XTAL1
// Input pull down
// RTC_CAL / OUT_CAP / LCDCTRL_nRST / BOOT_FORCE / LCDCTRL_POWER / LCDCTRL_SPI_NSS / LCDCTRL_SPI_SCK / LCDCTRL_SPI_MISO / LCDCTRL_SPI_MOSI / IN_CAP / I2C_SCL_ISO / I2C_SDA_ISO / NFC_POW
GPIO_InitStructure.Mode = GPIO_MODE_INPUT;
GPIO_InitStructure.Pull = GPIO_PULLDOWN;
GPIO_InitStructure.Pin = GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_2 | GPIO_PIN_6 | GPIO_PIN_7 | GPIO_PIN_8;
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
// Input pull up
// I2C_SCL / I2C_SDA / UART_RX / UART_TX / LPUART_TX / ISO_GPO
GPIO_InitStructure.Mode = GPIO_MODE_INPUT;
GPIO_InitStructure.Pull = GPIO_PULLUP;
GPIO_InitStructure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_8 | GPIO_PIN_9;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_4 | GPIO_PIN_5;
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
// Input no pull
// Analog
// PA7 / PB0 / PB1 / PB3 / PB9 / PB10 / PB11 / PB14 / PB15
GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Pin = GPIO_PIN_7;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_3 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_14 | GPIO_PIN_15;
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
}
2022-08-22 6:04 AM
Hello,
Two things here in my mind
Again the problem you faced is typical of an IO set as input and no pull is present.
Regards
Laurent
2022-08-22 6:42 AM
Hello,
It's working with the first remark, thank you ! I does not know that "normal state" init override "sleep state" init.
Regards,
Jean
2022-08-22 6:45 AM
Hello Jean,
Good to read.
Please tag this request as answered if you don't mind.
Regards
Laurent