2023-11-30 9:31 PM
Hello Team,
I am currently working with B-L475E-IOT01A2 for driving a "Waveshare" board "e-Paper IT8951 Driver HAT (B)" for updating E paper display. I am using SPI protocol for the same. I am trying to update the image but only 25% of the board is getting updated. Has someone faced same issue ? All the connections are proper, but the image is not getting fully updated.
I request and hope to hear soon. Thank you in advance.
Regards,
Amey Vandre
2023-12-04 2:14 AM
Well, you haven't given any indication of which software you are working with. Is it the example from the Waveshare website?
Regards
/Peter