2020-05-31 10:24 AM
Our test eeprom code taken from samples codes with address
Flash begin address 10040000 worked but not getting reprogram until boot pin gnd to 3.3v then gnd.
Flash address 10042850 is working but creating problem to reprogram
Then we tried 1007000,10060000, 1005000 not worked.
To program we hav to grd boot pin then high sort of reset then only we are able to program..n by doing this we r able to make our code work once for that 10042850 flash address n not for other values..either boot pin reset is not taking place or v r doing smething wrong while choosing flash addressess.
/******************** (C) COPYRIGHT 2015 STMicroelectronics ********************
* File Name : Flash/DataStorage/main.c
* Author : RF Application Team
* Version : V1.0.0
* Date : September-2015
* Description : Code demostrating the Flash functionality
********************************************************************************
* THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS
* WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE TIME.
* AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY DIRECT,
* INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING FROM THE
* CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE CODING
* INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.
*******************************************************************************/
/* Includes ------------------------------------------------------------------*/
#include "bluenrg_x_device.h"
#include "BlueNRG1_conf.h"
#include "SDK_EVAL_Config.h"
#include <stdio.h>
/** @addtogroup BlueNRG1_StdPeriph_Examples
* @{
*/
/** @addtogroup Flash_Examples
* @{
*/
/** @addtogroup Flash_DataStorage Flash Timer Example
* @{
*/
#define FLASH_START (_MEMORY_FLASH_BEGIN_)
#define FLASH_END (_MEMORY_FLASH_END_)
#define IS_FLASH_ADDRESS(ADDR) ( ((ADDR) >= FLASH_START) && ((ADDR) <= FLASH_END) )
#define N_BYTES_WORD (4)
#define N_ROWS (8)
#define N_BYTES_PAGE (_MEMORY_BYTES_PER_PAGE_)
#define N_PAGES (_MEMORY_FLASH_SIZE_/N_BYTES_PAGE)
#define N_WORDS_ROW (N_BYTES_PAGE / N_ROWS / N_BYTES_WORD)
#define N_WORDS_PAGE (N_BYTES_PAGE / N_BYTES_WORD)
#define IS_PAGE_NUMBER(PAGE) ( (PAGE)<N_PAGES )
#define IS_ROW_NUMBER(ROW) ( (ROW)<N_ROWS )
#define IS_WORD_NUMBER(WORD) ( (WORD)<N_WORDS_PAGE )
/* Remap values for the vector table. CONFIG register */
#define FLASH_REMAP_RAM 0x02
#define FLASH_PREMAP_MAIN 0x08
/**
* @brief User FLASH base address
*/
#define _MEMORY_FLASH_BEGIN_ 0x10040000
#define _MEMORY_FLASH_SIZE_ 0x40000 /* 256KB */
#define _MEMORY_FLASH_END_ 0x1007FFFF
#define _MEMORY_BYTES_PER_PAGE_ (2048)
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
#define DATA_STORAGE_PAGE (N_PAGES-8)
#define DATA_STORAGE_ADDR (((N_PAGES-8)*N_BYTES_PAGE) + FLASH_START)
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
char message[] = "BlueNRG-1 Flash Example - DATA STORAGE";
/* Private function prototypes -----------------------------------------------*/
/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program code
* @param None
* @retval None
*/
int main(void)
{
uint32_t memory_word = 0;
uint8_t message_length = sizeof(message);
uint8_t number_of_words = ((message_length / N_BYTES_WORD) + 1) * N_BYTES_WORD;
/* System initialization function */
SystemInit();
/* Identify BlueNRG1 platform */
SdkEvalIdentification();
/* UART initialization */
SdkEvalComUartInit(UART_BAUDRATE);
/* LEDs initialization function */
SdkEvalLedInit(LED1);
/* Flash - Data Storage example */
printf("******************************\r\n* Flash - Data Storage example\r\n******************************\r\n");
/* Erase the DATA_STORAGE_PAGE before write operation */
FLASH_ErasePage(DATA_STORAGE_PAGE);
/* Wait for the end of erase operation */
while(FLASH_GetFlagStatus(Flash_CMDDONE) != SET);
/* Erase page success */
printf("Page %d erased.\r\n", DATA_STORAGE_PAGE);
/* Write and verify operation */
printf("Write message: \"%s\"\r\n", message);
for(uint8_t i = 0; i < number_of_words; i++) {
memory_word = 0;
for(uint8_t j = 0; j < 4; j++) {
if( ((i*4)+j) > message_length) {
memory_word |= (uint32_t)(0xFF<<(8*j));
}
else {
memory_word |= (uint32_t)(message[i+j]<<(8*j));
}
}
/* Program the word */
FLASH_ProgramWord(DATA_STORAGE_ADDR + (i*4), memory_word);
/* Wait for the end of write operation */
while(FLASH_GetFlagStatus(Flash_CMDDONE) != SET);
printf("Write at address: 0x%08X. ", DATA_STORAGE_ADDR + (i*4));
/* Verify operation */
if( memory_word != FLASH_ReadWord(DATA_STORAGE_ADDR + (i*4)) ) {
printf("Verification failed 0x%08X.\r\n", (int)FLASH_ReadWord(DATA_STORAGE_ADDR + (i*4)));
while(1);
}
else {
printf("Success.\r\n");
}
}
SdkEvalLedOn(LED1);
/* Infinite while loop */
while (1);
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
/**
* @}
*/
/**
* @}
*/
/**
* @}
*/
/******************* (C) COPYRIGHT 2015 STMicroelectronics *****END OF FILE****/
can any please help i want to save 6 uint32_t data type variable in internal flash of bluenrg 232 SOC. How can i do that i am taking the above code as sample code for saving .