2019-07-29 8:42 AM
Hi all,
I am using a Nucleo-144 board and enabled the FreeRTOS. Afterwards i've integrated FreeRTOS+TCP sources and headers and Paho MQTT application.
I created a thread to run a MQTT Echo Server but i am having troubles connecting. This is my code:
static void prvMQTTEchoTask(void *pvParameters)
{
printf("prvMQTTEchoTask\n\r");
/* connect to m2m.eclipse.org, subscribe to a topic, send and receive messages regularly every 1 sec */
MQTTClient client;
Network network;
unsigned char sendbuf[80], readbuf[80];
int rc = 0,
count = 0;
MQTTPacket_connectData connectData = MQTTPacket_connectData_initializer;
pvParameters = 0;
NetworkInit(&network);
printf("Network Initialized\n\r");
MQTTClientInit(&client, &network, 30000, sendbuf, sizeof(sendbuf), readbuf, sizeof(readbuf));
printf("MQTT Client Initialized\n\r");
//char* address = "iot.eclipse.org";
char* address = "0.0.0.0";
if ((rc = NetworkConnect(&network, address, 1883)) != 0)
printf("Return code from network connect is %d\n\r", rc);
#if defined(MQTT_TASK)
printf("MQTTStartTask\n\r");
if ((rc = MQTTStartTask(&client)) != pdPASS)
printf("Return code from start tasks is %d\n\r", rc);
#endif
connectData.MQTTVersion = 3;
connectData.clientID.cstring = "FreeRTOS_sample";
printf("Connection Attempt...\n\r");
if ((rc = MQTTConnect(&client, &connectData)) != 0)
printf("Return code from MQTT connect is %d\n\r", rc);
else
printf("MQTT Connected\n");
if ((rc = MQTTSubscribe(&client, "FreeRTOS/sample/#", 2, messageArrived)) != 0)
printf("Return code from MQTT subscribe is %d\n\r", rc);
while (++count)
{
MQTTMessage message;
char payload[30];
message.qos = 1;
message.retained = 0;
message.payload = payload;
sprintf(payload, "message number %d", count);
message.payloadlen = strlen(payload);
if ((rc = MQTTPublish(&client, "FreeRTOS/sample/a", &message)) != 0)
printf("Return code from MQTT publish is %d\n\r", rc);
#if !defined(MQTT_TASK)
if ((rc = MQTTYield(&client, 1000)) != 0)
printf("Return code from yield is %d\n\r", rc);
#endif
HAL_Delay(5000);
}
/* do not return */
}
I've tried passing an ip address or a name like "localhost" but it keeps giving me an error code at this point:
if ((rc = NetworkConnect(&network, address, 1883)) != 0)
printf("Return code from network connect is %d\n\r", rc);
Any suggestion? Thank you.
2019-07-30 2:34 AM
I realized that i don't have any address set up, by running:
FreeRTOS_GetAddressConfiguration( &ulIPAddress,
&ulNetMask,
&ulGatewayAddress,
&ulDNSServerAddress );
/* Convert the address to a string then print it out. */
FreeRTOS_inet_ntoa( ulIPAddress, cBuffer );
printf("IP Address: %s\r\n", cBuffer);
FreeRTOS_inet_ntoa( ulNetMask, cBuffer );
printf( "Subnet Mask: %s\r\n", cBuffer );
FreeRTOS_inet_ntoa( ulGatewayAddress, cBuffer );
printf( "Gateway Address: %s\r\n", cBuffer );
FreeRTOS_inet_ntoa( ulDNSServerAddress, cBuffer );
printf( "DNS Server Address: %s\r\n", cBuffer );
I print :
IP Address: 0.0.0.0
Subnet Mask: 0.0.0.0
Gateway Address: 0.0.0.0
DNS Server Address: 0.0.0.0
2019-07-30 8:18 AM
I modified the code and now i print different stuff:
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals /
MX_GPIO_Init();
MX_ETH_Init();
MX_USART3_UART_Init();
MX_USB_OTG_FS_PCD_Init();
/ Initialise the RTOS’s TCP/IP stack. The tasks that use the network
are created in the vApplicationIPNetworkEventHook() hook function
below. The hook function is called when the network connects. */
FreeRTOS_IPInit( ucIPAddress,
ucNetMask,
ucGatewayAddress,
ucDNSServerAddress,
ucMACAddress );
uint32_t ulIPAddress, ulNetMask, ulGatewayAddress, ulDNSServerAddress;
int8_t cBuffer[ 16 ];
/* Create the thread(s) /
/ definition and creation of defaultTask /
//osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
//defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
vStartMQTTTasks(ipconfigIP_TASK_STACK_SIZE_WORDS, 0);
/ USER CODE BEGIN RTOS_THREADS /
/ add threads, ... /
/ USER CODE END RTOS_THREADS /
/ The network is up and configured. Print out the configuration
obtained from the DHCP server. */
FreeRTOS_GetAddressConfiguration( &ulIPAddress,
&ulNetMask,
&ulGatewayAddress,
&ulDNSServerAddress );
/* Convert the address to a string then print it out. */
FreeRTOS_inet_ntoa( ulIPAddress, cBuffer );
printf("IP Address: %s\r\n", cBuffer);
FreeRTOS_inet_ntoa( ulNetMask, cBuffer );
printf( "Subnet Mask: %s\r\n", cBuffer );
FreeRTOS_inet_ntoa( ulGatewayAddress, cBuffer );
printf( "Gateway Address: %s\r\n", cBuffer );
FreeRTOS_inet_ntoa( ulDNSServerAddress, cBuffer );
printf( "DNS Server Address: %s\r\n", cBuffer );
/* Start scheduler /
//osKernelStart();
vTaskStartScheduler();
/ We should never get here as control is now taken by the scheduler */
/* Infinite loop /
/ USER CODE BEGIN WHILE */
while (1)
{
}
/* USER CODE END 3 */
}
Those printfs give me the following prints:
IP Address: 0.0.0.0
Subnet Mask: 255.255.255.0
Gateway Address: 10.9.23.1
DNS Server Address: 10.9.3.43
Since i initialized the arguments given to FreeRTOS_IPInit as :
static const uint8_t ucIPAddress[ 4 ] = { 10, 9, 23, 44 };
static const uint8_t ucNetMask[ 4 ] = { 255, 255, 255, 0 };
static const uint8_t ucGatewayAddress[ 4 ] = { 10, 9, 23, 1 };
static const uint8_t ucDNSServerAddress[ 4 ] = { 10, 9, 3, 43 };